Error Management
When a non-fatal error occurs and motion must be stopped quickly these procedure can be taken:
Axis Procedures
|
Step |
Example Application Code |
|---|---|
|
Send Stop Command for each axis. |
(PipeNetwork.AXI_A1_Axis, TRUE, DEF_A1_StopDec); |
|
Stop the Axis Motion Generator. |
(PipeNetwork.AXI_A1_Axis, 0.0); |
|
Wait for Axis to be stopped. |
AxisStatus := MLAxisStatus (PipeNetwork.AXI_A1_Axis); (PipeNetwork.AXI_A1_Axis,FALSE,DEF_A1_StopDec); |
|
Turn power off(disable) all the axes. |
(PipeNetwork.AXI_A1_Axis,FALSE); |
|
Disconnect Pipe Network from the axis. |
(PipeNetwork.CNV_A1); |
Machine Procedures
|
Step |
Example Application Code |
|---|---|
|
Stop Command at the master block level. |
(PipeNetwork.MASTER, 0.0); |
|
Wait for Master command to be stopped. |
IF A1_AckState = DEF_StateErrorStop |
-
- This code is only applicable to Pipe Network applications.
It does not work in a PLCopen application.
This procedure for error management is based on the Project Structure Guidelines described in Application Software Structure - Implementation.
See Restarting Motion with Pipe Network about restarting the motion.